Instructions
Enter data in the fields provided. If an input is out of range an alert will appear.
Click "Update" or tab to another field to see node voltages annotate the schematic on the right.
If the combination of inputs causes internal or external limits to be exceeded, the problem node value will be highlighted in red and an "Out of Range!" message will appear. When this message is present, all node values should be considered invalid.
Only one of "Gain" or "RG" can be specified - the other is computed automatically.
|