Troubleshooting Guide: Assistance for problems using Interactive Tools
General
This website as a whole and Interactive Tools in particular requires a DHTML-compliant, JavaScript-enabled browser, such as Microsoft Internet Explorer 5.0 (or more recent) or Netscape 7.1. In addition to JavaScript, some tools require the presence of a JDK 1.1-compliant Java Virtual Machine (JVM), either built-in to the browser or installed as a plug-in. Despite the similarity in their names, Java and JavaScript are separate, unrelated technologies and enabling one does not do anything for the other. A third necessary technology required for some tools is something called LiveConnect, which allows Java and JavaScript to exchange information.
If you see a green "JavaScript is enabled." above and at least one green "Java with LiveConnect is working" message, you should be able to use Interactive Tools. Select your browser from the pull-down menu and click "Go" for instructions on how to enable your browser for these technologies if they are not currently enabled.
Known Limitations
The tools are tested to work with Windows browsers only. On other platforms, the most recent version of Netscape or IE is recommended.
Netscape Navigator 4 is no longer officially supported and has known bugs with respect to window resizing and DHTML layers. Some resizing problems are automatically detected and will reload the page when they occur. Unfortunately, entered form data may be lost.
Enabling Java and JavaScript - Tools: Internet Options: Security
From the Tools menu, select Internet Options... and then the Security panel. Ordinarily, the Analog website will be assigned to the Internet web content zone with a security level of "Medium". JavaScript can only be disabled using a Custom security configuration. To enable JavaScript first click "Custom Level..." and then "Enable Active Scripting", located within the "Scripting" section of the Custom Level window. (Always consult your System Administrator before changing browser security settings)
If the security level is set to "High", some key features - such as Active Scripting, Scripting of Active X controls and Java applet scripting - may be disabled. The symptom of the last two being disabled is the somewhat obtuse error alert "An ActiveX control on this page is not safe..." displayed over a running applet. These features can be manually enabled (while leaving all other security settings at High) by clicking "Custom Level", resetting the configuration to "High security", and then enabling just JavaScript ("Enable Active Scripting"), "Script ActiveX Controls Marked Safe for Scripting" (in the "ActiveX controls..." section) and "Scripting of Java Applets" (in the "Scripting" section). For IE6 you may also have to enable Java applets as well ("Microsoft VM : Java Permissions").
If Java itself doesn't work there are two main causes: 1) that it was never installed or 2) that it has been disabled. Java can be disabled by means of a Custom Security configuration. To enable Java, select "High safety" from the "Microsoft VM : Java Permissions" section of Custom Security settings. The symptom is the same error alert "An ActiveX control on this page is not safe..." mentioned above, except in this case the applet does not run.
If there is no "Microsoft VM" section under Custom settings, Java is not installed and this can be confirmed by checking the Advanced panel, which will also have no "Microsoft VM" section. The symptom in this case is a broken plug-in icon in a gray box where the applet should be. Although you may see a dialog offering to download Microsoft's version of Java it is no longer available from Microsoft's website and you should consider installing Sun Microsystem's Java 2 plug-in instead (about an 8MB download); see the instructions below.
Netscape 4 is no longer supported, and users of Netscape 4 should consider upgrading to Netscape 7.1 or the latest version of Mozilla, for compatibility and security reasons. In particular, please note that Netscape 4 will no longer work for all Java-based tools when accessed behind a firewall-proxy without DNS support. Newer tools also require more DHTML support than is available in Netscape 4.
If you are using any version of Netscape 6 we recommend updating to Netscape 7.1 or the latest version of Mozilla (currently 1.4) for maximum compatibility with Analog's Interactive Tools.
Enabling Java and JavaScript - Edit: Preferences: Advanced
From the Edit menu, select Preferences... and then the "Advanced" category. For Netscape 6, it is not necessary to open the sub-categories under Advanced - selecting "Advanced" itself will bring up a panel from which both Java and JavaScript can be enabled or disabled. For Netscape 7, Java can still be enabled or disabled at the top level, but to enable/disable JavaScript one must click on the subcategory "Scripts & Plugins". "Enable native object scripting" should also be checked (next to "Enable Java"). Java, JavaScript and native object scripting should be enabled for maximum compatibility with Analog Devices tools. It is not necessary to enable JavaScript for Mail & Newsgroups.
The default ("Recommended") download installation of Netscape 7 does NOT include Java, which must be downloaded and installed separately. Selecting the "Full" Netscape 7 installation option DOES include Java.
Macintosh browsers are not supported, however, the most recent browser versions (such as IE 5.5 with Apple's Java interpreter) should work for most applets.
The latest version of Opera, 7.23, is the version most compatible with Analog's Interactive Tools.
Analog's Java-based tools first try to use whatever Java Run Time is the default for the browser. If that is unavailable, they expressly try to use a plug-in Java Virtual Machine (JVM). If no Java intepreter is found, recent versions of Internet Explorer, Netscape, Mozilla and Opera should prompt for Java installation. Unfortunately, IE may try to install its own "Microsoft Virtual Machine" (MVM), which is no longer supported by or available from Microsoft. If automatic Java installation doesn't work, the plug-in can be downloaded and installed from Sun's plug-in site. Follow the instructions given in the installation process.
For IE5+, NS7 and Mozilla, the Java Plug-in Control Panel allows you to choose the default java interpreter for your browser (under "Browser"), and even which version to use if you happen to have multiple versions installed (under "Advanced"). Also, if you have multiple JVM's installed, you can select which one is active. Always check with your System Administrator to make sure that altering these settings won't interfere with other applications.
Special requirements for Sun Java plug-in use:
Internet Explorer 4-6
Under Security, "Run ActiveX controls and plug-ins" must be enabled, as should "Script ActiveX controls marked safe for scripting". These settings are automatically enabled when "Medium" or "Low" security is selected. "High" security settings will need to be customized (see above). To use the plug-in for all applets, "Use Java 2..." must be checked under "Java (Sun)" in the Advanced panel.
Other Browsers
User of non-Microsoft browsers may require setting "-DtrustProxy=true" in the Java Runtime Parameters, located within the Advanced tab of the Java Plug-in control.
Netscape 4.X
Later versions (4.78+) of Netscape 4 specially recognize the Java plug-in and provide a separate checkbox in the Advanced settings to enable and disable it. If both the regular VM and plug-in are installed and this box is checked, the plug-in Java interpreter will be used. If the box is unchecked, the built-in interpreter is used. If the plug-in is installed and no internal JVM is found, the plug-in is used. However, plug-in Java is incompatible (in Netscape 4) with LiveConnect scripting, preventing some calculator features from working.
Legal Disclaimer:
Information furnished by Analog Devices is believed to be accurate and reliable. However, no responsibility is assumed by Analog Devices for its use, nor for any infringements of patents or other rights of third parties which may result from its use. No license is granted by implication or otherwise under any patent or patent rights of Analog Devices.