Instructions
This tool computes idealized values for gain, output voltage and DC transfer characteristics of the AD8330, given the input control voltages and load resistances.
To use this tool, enter application parameters in the fields provided at left. Hit Enter or click Calculate to accept the entries and perform the calculations. The AD8330's gain is exponentially dependent on VDBS (relative to VCMG), linearly dependent on VMAG (relative to VCMG) and the differential input voltage (VIN), and produces differential outputs, VOPHI and VOPLO that are symmetrical about VCNTR, which may be also be changed, but by default is centered between the supply voltages, VS and VCOMM. Inverting mode for VDBS may be selected via the mode pulldown.
A sample output voltage may be calculated by entering a value in VIN with the result shown in VOUT. Supply limits and source (RS) and load (RL) impedances affect VOUT, but do not affect the idealized gain.
A chart is shown at upper left of this tool. Two plots are available: the default plot is of ideal gain vs VDBS, ignoring limits set by Vin, Vmag and the supply voltages.
The other plot shows VOPHI and VOPLO vs. VIN, taking these limits into account. Parametric variations in gain are not taken into account in this tool.
Quantities in gray-outlined boxes cannot be changed. Out-of-range and other error messages are flagged in a yellow message field at the bottom of the calculator.
Note: This tool only supports a single positive supply voltage (VS) for input, internal and output supplies.
|