Overview:
The purpose of this tool is to help with the selection, evaluation and
troubleshooting of voltage feedback operational amplifiers (Op-Amps). It uses
typical parametric data to mathematically model the general behavior of a
selected amplifier. It allows a user to select an amplifier, quickly configure
a circuit, apply a signal and evaluate the general performance. It is useful
for checking an amplifier's parametric performance such as Gain Bandwidth, Slew
Rate, Input/Output Range, Differential Voltages, Gain Error, Load Current,
Possible Stability Issues and DC Errors in a given circuit configuration. This
tool is limited to first order approximations and should not be used in place
of SPICE modeling or hardware testing.
Select Amplifier | Select
the Circuit | Configure the Circuit |
Input Signal | Analyze the Amplifier
Response
How to use the tool:
Select Amplifier
Choose an Amplifier to be evaluated from the pull down, labelled "Select
Amplifier," located at the top of the tool. Additional amplifiers can be added
to the list by using one of the options below:
-
Parametric Search
- If you know the required op-amp parameters the Parametric Search Engine can
be used to find and suggest amplifiers for evaluation. To perform a
search enter the values for the desired parameters in the input blocks provided
and press search. The tool will display results that best meet the input
criteria. Additional search parameters can be added by checking the desired box
under "Add Searchable Parameters". If desired, amplifiers can be selected
for further evaluation by selecting the Add Part(s) to Amplifier Parametric
Evaluation Tool, selecting the checkbox next to the desired part(s), then
clicking the Add to Tool button at the bottom of the page.
-
Amplifier Wizard
- If you're not sure of how to select an amplifier, let the Amplifier Wizard
help suggest one. The Amplifier Selection Wizard will lead you through a
few generic questions and based on the response information will search for and
sugest amplifiers for further evaluation.
-
Reverse Search - Data derived from the configured circuit can
be used to automatically load the parametric search engine. This allows the
parametric search to look for an amplifier that will work in the circuit. If an
amplifier that meets all requirements can't be found the search will suggest
components that are close.
Select the Circuit
Choose the a circuit from the pull down, labelled "Select Mode," located at the
top of the tool. The selections are Inverting amp, Non-Inverting amp or
Difference amp configurations.
Configure the Circuit
Set the Gain
Adjusting the ratio of Rfb/Rg set the closed loop gain. Enter values for the
resistors in the input blocks provided.
(Note: Large resistance values will increase errors due to
input bias current and voltage noise)
Enter the Power Supply Voltages
Enter the desired Power Supply Voltage in the +Vsupply and -Vsupply input blocks
provided.
Source Resistance
Enter the input signal source resistance in the block provided. The default
resistance is 0 ohms. Large source resistances will increase errors due to
input bias current and voltage noise.
Vref
A reference Voltage may be entered in the in the Vref block provided. The
default value for Vref is 0 Volts. The Vref. voltage is used to perform level
shifting of the signal.
Rbias Resistor (Inverting and Non-Inverting Modes only)
If desired enter a value for the Rbias resistor in the block provided.
(Note: In the Non-Inverting Mode Rbias resistance must be
greater than 0 Ohms or the input signal will be shorted to Vref. The Rbias is
used with non bias compensated op-amps to minimize errors due to input bias
current. It does so by matching the source impedance seen at the non-inverting
(+) pin to that seen by the inverting (-) pin. The value of Vbias is generally
set to match the parallel resistance of Rfb//Rg.)
Rload
Resistive Loading of the Amplifier's Output can be set by entering a value for
Rload in the block provided. The default value is 1 Gig. Ohms
(Note: Low resistance values can cause the output of the
op-amp to draw excessive current)
Cload
Capacitive Loading of the Amplifier's Output can be set by entering a value for
Cload in the block provided. The default value is 1 pF.
(Note: Large capacitance values can cause an op-amp to become
unstable or draw high output current when used with a signal that has
frequency.)
Back to top
Input Signal
Select Input Signal
Choose the Input Signal Waveform from the pull down, labelled "Input Signal,"
located just above the graph at the left. The available selections are Sine,
Triangle and DC.
Setting the Frequency
Enter the desired Input Signal Frequency in the block provided.
(Note: This block is not shown for DC.)
Setting the Amplitude
Enter the desired Voltage Input Signal Amplitude in the block provided.
(Note: This block is not show when DC is selected, use the DC
Offset block to set the Amplitude.)
Setting the DC Offset
The DC offset block is used to set the DC Offset Voltage applied to the Input
Signal. In the Differential Mode this sets the average DC Voltage difference
between Input Signals V2 and V1.
Setting the Common Mode Voltage (Differential Mode only)
The Common Mode Voltage block is used to set the Average DC Voltage value of
Input Signals V1 and V2.
Back to top
Analyze the Amplifier Response
Running The Model
To Run the Model click on the Run Model button located at the
upper right of the tool.
(Note: Each time a change is made the model will need to be
manually re-run.)
Viewing Results
The calculated response for the selected amplifier is displayed in a graph on
the lower right of the tool. Options for what is included in the displayed
waveform are located below the graph.
Gain Error
The radio buttons provided allow the user the option of Including or Excluding
gain error in the results graph. If Gain Error is excluded a caution flag will
be set when the total Gain Error and DC Errors exceed 1%. If Include is
selected the Gain error is included in the graph shown and in the gain block at
the Right and no caution flag will be set.
Gain
The Gain indicator displays either the Ideal Gain or the Actual Gain. The Ideal
Gain is defined by the values of the gain resistors. The Actual Gain is defined
by the values of the Gain resistors, Feedback Factor and the Open Loop Gain of
the selected amplifier at the defined input frequency.
DC Error
The radio buttons provided allow the user the option of Excluding or Including
+/- DC errors in the results graph. If DC Errors are excluded a caution flag
will be set when the total Gain Error and +/- DC Errors exceed 1%. If Include
is selected the DC error is included in the graph shown
Output Voltage
A Digital Volt Meter (DVM) function is provided to assist in reading the Graph
Voltages. The DVM functions Volts peak to peak V(P-P), Volts RMS V(RMS) and
Volts DC V(DC).
Log Box
Located below the response graph at the lower right is a log box. It displays
detected faults in 2 levels of error, Alerts and Cautions.
Alert
Alerts are used to flag and detail conditions under which the selected amplifier
should never be operated. When an Alert flag appears in the log box no response
is shown in the display graph and corrective actions must be taken before the
display will show a response. Conditions that can cause an Alert include
exceeding the absolute maximums for the device or possible oscillations.
Suggested solutions for resolving alerts follow the Alert details.
Caution
Cautions are used to flag and detail conditions for which the selected amplifier
is being operated outside it's typical performance range. When a Caution flag
appears in the log box a typical first order response (derived from parametric
data) is shown in the display graph. Conditions that can cause a Caution
include exceeding the selected amplifier's useable input range, output range,
slew rate or bandwidth. Suggested solutions for resolving cautions follow the
caution details.
Back to top
|